Reply
Posts: 36
Registered: ‎06-13-2013

Quick Links for Unread Posts

[ Edited ]

 

Below are the direct links for specific boards, or to the unread content on those boards. For frequent visitors to the site, it is sometimes easier to jump directly to new unread content.  We hope that these links will help you find what you need faster.

 

TO USE THE LINKS: 

 

The bold item is the direct board URL, and the longer URL is the link to the unread content on that board. 

 

Just click on the board title to jump directly to that forum content ... then create a shortcut in your browser that you can use later to come back to the same area.

 

The “new unread content” URL is more complex in its construction, but it works the same way.  Just click the link and create your bookmark. 

 

Don't forget that once you read content, you will probably not see it again under the "unread" category.  So both links might prove helpful.

 

If you need to login again after clicking directly into the forum, you might consider checking the "keep me signed in" option when you enter your credentials.

 

Feedback is welcome. 

Thanks

 

 

8-Bit Discussion:                        http://community.silabs.com/t5/forums/unreadpostspage/board-id/1/post-type/message

32-Bit Discussion:                      http://community.silabs.com/t5/forums/unreadpostspage/board-id/2/post-type/message

Microcontroller How-to Guideshttp://community.silabs.com/t5/forums/unreadpostspage/board-id/3/post-type/message

Wireless Discussion:               http://community.silabs.com/t5/forums/unreadpostspage/board-id/4/post-type/message 

Sensor Discussion:                   http://community.silabs.com/t5/forums/unreadpostspage/board-id/Sensor_Area/post-type/message

Timing Discussion:                   http://community.silabs.com/t5/forums/unreadpostspage/board-id/Timing_Discussion/post-type/message

Interface Products:                    http://community.silabs.com/t5/forums/unreadpostspage/board-id/5/post-type/message

Simplicity Studio and Software Toolshttp://community.silabs.com/t5/forums/unreadpostspage/board-id/6/post-type/message

Hardware Tools:                   http://community.silabs.com/t5/forums/unreadpostspage/board-id/Hardware_Tools/post-type/message

Tools - Beta Releases:         http://community.silabs.com/t5/forums/unreadpostspage/board-id/Tools_Beta_Releases/post-type/message

Community Submitted Projectshttp://community.silabs.com/t5/forums/unreadpostspage/board-id/9/post-type/message

Contests:                               http://community.silabs.com/t5/forums/unreadpostspage/board-id/8/post-type/message

Feedback and Ideas:            http://community.silabs.com/t5/forums/unreadpostspage/board-id/10/post-type/message

 

Moderators only:

Abuse Board:                                    http://community.silabs.com/t5/forums/unreadpostspage/board-id/AbuseBoard/post-type/message

Posts: 3,150
Registered: ‎02-07-2002

Re: Quick Links for Unread Posts

And how does this work for the Knowledge Base? That is the only one that often indicates there are new messages without having a new message at the top of my list.

Posts: 203
Registered: ‎02-04-2013

Re: Quick Links for Unread Posts

Is there a way to navigate to the 'new unread content' page from the regular board? I can create bookmarks, but i'm sure for some people who only need that view from time to time being able to navigate there normally would be nice. 

----------------------------
Josh Norem
Senior Applications Engineer
Silicon Labs
Posts: 3,150
Registered: ‎02-07-2002

Re: Quick Links for Unread Posts


vanmierlo wrote:

And how does this work for the Knowledge Base? That is the only one that often indicates there are new messages without having a new message at the top of my list.


Any news on this? I once again seem to have 9 unread messages in the KB, but I can't find them.

Posts: 4
Registered: ‎01-13-2015

Re: Quick Links for Unread Posts

Is there by any chance a way to search for messages which have no replies, rather than ones that are unread?  It seems this would be useful if users want to be helpful and find posts where they could potentially contribute answers.

 

Greg

Administrator
Posts: 677
Registered: ‎09-04-2012

Re: Quick Links for Unread Posts

[ Edited ]

Hi, Greg 

 

Yes you can. If you go to the Search page and choose 'Advanced Search', you'll see more options including 'Topics with no replies'.

http://community.silabs.com/t5/forums/searchpage/tab/message?filter=labels

 

You can choose other options like filtering content by type of post ect. afterwards. Please let me know if you have any other question. 

 

topics with no replies.png


Nari | Community Manager | Silicon Labs
Highlighted
Posts: 3,150
Registered: ‎02-07-2002

Re: Quick Links for Unread Posts

[ Edited ]

For the Other Products forum:

Other-Products: http://community.silabs.com/t5/forums/unreadpostspage/board-id/Everything_else_Silicon_Labs/post-typ...

 

Unfortunately it doesn't always work. As at this moment I seem to have 4 unread messages here, but the above link shows none.