Reply
Highlighted
Posts: 36
Registered: ‎06-13-2013

Help Topic: Enabling Chroma Formatting for Code

[ Edited ]

Did you know that code within your posts can be colored for easier reading?  It's easy to do. 

 

Start your post however you like.  When you're ready to add your programming code ... Just click the code entry button (the clipboard with the 'C' shown below) and insert your code into the pop-up window.  Click insert on the pop-up window to complete the action

 

code_insert_button.gif

 

#include<stdio.h> 
int main()
{
  printf(“Hello World\n”);
  return 0;
}