Reply
Highlighted
Posts: 119
Registered: ‎05-30-2012

Overview of ZigBee Connected Home Reference Designs

  

Agenda

 

Learn more about the reference design here.

 

What is ZigBee?

 

ZigBee is the wireless language that everyday devices use to connect to one another. ZigBee harnesses the power of the mesh to connect every product to every other product. So if one of your products fails, the others will continue to communicate without interruption. ZigBee standardizes everything from basic communication to how a product operates. Products with the ZigBee logo work together seamlessly, even if they’re from different companies. ZigBee allows devices to last for years on a single battery.

 

Silicon Labs Ember® is the platform of choice for OEMs developing ZigBee networking into their products. The Ember ZigBee platform is the most integrated, complete and feature rich ZigBee solution available — a single-chip, high-performance 2.4 GHz ZigBee transceiver and ARM Cortex-M3 processor integrated with the most reliable, scalable and advanced ZigBee PRO software and supported by best-in-class development tools.

 

Learn more on www.silabs.com

Posts: 8
Registered: ‎05-04-2015

Re: Overview of ZigBee Connected Home Reference Designs

Hi 

    I do not know why i can't watch video files.

Administrator
Posts: 884
Registered: ‎12-03-2014

Re: Overview of ZigBee Connected Home Reference Designs

HI, @Alenix52

 

You may not be able to see the video if you are based in China as it is hosted by Youtube which is blocked in China. 

 

If that's the case, you can watch the same video in Youku: http://v.youku.com/v_show/id_XMTM4OTA3NDYzNg==.html?from=y1.7-2

 

Let us know if it works for you. 

Silicon Labs Ember 是 OEM 在利用 ZigBee 网络开发产品时的首选平台。Ember ZigBee 平台是可用的集成度最高、最完善和功能丰富的 ZigBee 解决方案 - 一个单芯片、高性能 2.4 GHz ZigBee 收发器和 ARM Cortex-M3 处理器,与最可靠的、可扩展的先进 ZigBee PRO 软件集成,由最优的开发工具提供支持。http://www.silabs.com/iot/Pages/zigbee-connected-home-reference-designs.aspx