Reply
Administrator
Posts: 833
Registered: ‎12-03-2014

Creating an example EmberZNet Network

[ Edited ]

 

This video describes how to create a simple ZigBee Z3 light and switch network using Simplicity Studio and the Silicon Labs EmberZNet ZigBee protocol stack.

 

The example applications use touchlink commissioning to form the network. The light acts as the Touchlink target and the switch performs Touchlink commissioning to establish itself on the same network as the light. Once the network is formed you can use a button on the switch to toggle the light LED, and observe the interaction on a console interface to the devices.

 

Watch More Videos: 

 

Setting up EFR32 Development Kit Hardware

Installing Simplicity Studio for EFR32 Development Kits

  • You are here:  Creating an example EmberZNet Network

 

Learn More