Reply
Posts: 2
Registered: ‎07-21-2017

si5344: Error when Input freq 66.67MHz, Output Freq 10MHz with zero delay mode on

Hi All,

 

i'm having an error message below:

 

some of your manual N divider assignment are not valid because there are no common even multiples between all output frequencies across the N divider output range: -N0Robot surprisedUT2,OUT3

 

question:

-setting wrong?

- is there any setting that allow Input Freq 66.67MHz, Output Freq 10MHz with zero delay mode On?

 

 

please advise.

 

Thanks.

Highlighted
Posts: 1
Registered: ‎08-01-2017

Re: si5344: Error when Input freq 66.67MHz, Output Freq 10MHz with zero delay mode on

This was answered in salesforce ticket 00146691.