Reply
Highlighted
Posts: 2
Registered: ‎07-21-2014

What is the ESD class (HBM) for the Si4133?

 
Posts: 2,968
Registered: ‎02-07-2002

Re: What is the ESD class (HBM) for the Si4133?

Please do not double post.

Posts: 45
Registered: ‎02-24-2014

Re: What is the ESD class (HBM) for the Si4133?

The Si4133 is considered HBM Class 0B overall since the inductor pins passed 200V, all other pins passed 1000V.