Reply
Posts: 1
Registered: ‎09-20-2017

Si5383

Hi,

 

We are using SI5383 PLL in our Design. In this Recommended TCXO is not available.

Like T200F-012.8M of  Connor Winfield is Recommended and we are getting DV75C-012.8M of the same company . Is it suitable with Si5383PLL ?

 

Regards

Neelam

Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Star</font></font> </a> SPG
Posts: 1
Registered: ‎10-02-2017

Re: Si5383

You could contact Connor Winfield and ask if the DVC75C-012.8M MTIE TDEV performance is the same, or better, than the T200F series.