Reply
Posts: 1
Registered: ‎08-24-2017

Si5345A-D-GM Surface Finish

Hi, does anyone have details for the surface finish on the termination of Si5345A-D-GM? It doesn't look like the information is currently included in the Corporate, Product and Environmental Data.
Highlighted
Posts: 11
Registered: ‎06-18-2014

Re: Si5345A-D-GM Surface Finish

Per Salesforce Case 00149387:

 

The packaging engineer reported as follows.

 

    …The plating is actually part of the leadframe ...

 

    Plating is NiPd(Au-Ag).

 

    Based on the Homogeneous Material the masses are 1.250 mg Ni, 0.020 mg Au, 0.020 mg Ag.