Reply
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Super Star</font></font> </a> msb
Posts: 4
Registered: ‎09-11-2015
Accepted Solution

SI570, Can you precalcuate multiple frequencies and then change them without recalling the NVM?

We would like to precalculate approx 100 frequencies.  Can I calculate all my frequencies from doing only one reset or recall on the NVM then load them as need using the DCO freeze, load registers, unfreeze DCO, New Freq without doing a reset or recall NVM each time?

Highlighted
Posts: 45
Registered: ‎02-24-2014

Re: SI570, Can you precalcuate multiple frequencies and then change them without recalling the NVM?

Yes you can write the registers for each new frequency without first recalling the NVM. The DCO freeze operation allows direct writing of the frequency registers to the required values. DCO unfreeze + New Freq initiates the internal state machine to start using those register values in operation. An NVM recall operation is only needed if you want to return a device to factory settings.

 

Note that each Si570 device will have a slightly different internal crystal frequency so it is necessary to pre-calculate register values for each device separately for maximum frequency accuracy. You cannot use the internal crystal frequency of one device as the basis for calculating the register settings for other devices without having frequency offset errors. This is described in the Si570 datasheet.