Reply
Highlighted
Posts: 1
Registered: ‎05-02-2014

Can the Si53340 be used as a generic data buffer, rather than as a clock buffer?

[ Edited ]

Can the Si53340 be used as a generic data buffer, rather than as a clock buffer?  I see it has AC specs down to DC (i.e. not stopping at 1 MHz Min F like the 5330x.)  Its Any In - Any Out structure would be handy if so as a translator.

Posts: 87
Registered: ‎03-03-2014

Re: Can the Si53340 be used as a generic data buffer, rather than as a clock buffer?

The Si53340  input does not have to be a clock signal and a data input would be fine. You're correct, it does make a good logic translator!