Using the Si533xx buffer in a spread spectrum application

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> FranBoudreau on ‎05-28-2015 01:35 PM - edited on ‎12-02-2015 10:04 AM by Administrator Siliconlabs

Question

Can a Si533xx be used in a spread spectrum application?

Answer

The Si533xx buffer family does not incorporate a PLL and can be used in a spread spectrum application. This includes the Si53301. Si53302, Si53303, Si53304, Si53305, Si53306, Si53307, Si53308, Si53311, Si53312, Si53313, Si53314, Si53315, Si53320, Si53321, Si53322, Si53323, Si53324, Si53325, Si53340, Si53360 and Si53365.