Max Input VCM for the Si533xx buffer

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> FranBoudreau ‎04-06-2015 08:22 AM - edited ‎05-13-2015 09:40 AM

Question

What is the max VCM input for the Si533xx buffer?

Answer

The max VCM is VDD-0.9V