Reply
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Super Star</font></font> </a> fg
Posts: 7
Registered: ‎03-20-2017
Accepted Solution

using EFM32 Eval Board to debug EFR32

Hello,

 

I am currently developing with the EFR32 Flex Gecko on a custom PCB with the EFR32 Flex Gecko Eval Board as debugger/programmer.

Now I need more debuggers. Can I also use for example a EFM32 PEARL GECKO STARTER KIT (SLSTK3401A) for debugging or is this only possible with a EFR32 eval board?

 

Thanks for your help

Posts: 213
Registered: ‎12-05-2016

Re: using EFM32 Eval Board to debug EFR32

Hi @fg,

 

Good question! Yes an EFM32 eval board can be used to be the debug host for a custom EFR32 board.  The J-Link controller that is on the EFM32 STK gives the necessary functionality.

 

Thank you,

jpitt

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Super Star</font></font> </a> fg
Posts: 7
Registered: ‎03-20-2017

Re: using EFM32 Eval Board to debug EFR32

Hi @jpitt

 

perfect, that is the answer I was hoping to get.

Thank you!

Posts: 6
Registered: ‎11-20-2016

Re: using EFM32 Eval Board to debug EFR32

Does Thunderboard React only support 'out' in debugger mode? 

Thank you 

Highlighted
Posts: 1,735
Registered: ‎10-14-2014

Re: using EFM32 Eval Board to debug EFR32

@kimkyeyoung,
i am a little bit confused.
are you asking "does an j-link debugger was included in the thunderboard react kit"?
WeiguoLu