Reply
Posts: 11
Registered: ‎01-20-2017

experience in standard gcc compiler for SS4

Hello,

 

is anyone expierienced in using a standard gcc compiler to use for SS4 instead of keil and IAR?

which one can I use?

 

regards,

 

hobbit23

Posts: 2,890
Registered: ‎02-07-2002

Re: experience in standard gcc compiler for SS4

GCC is (can be) installed with SS4. But beware, not all SDK's support GCC (yet).

Posts: 11
Registered: ‎01-20-2017

Re: experience in standard gcc compiler for SS4

i am using the EFR32MG1P132F256GM48. can i switch the compiler somewhere to test if the (mabe) installed GCC is working?

Posts: 2,890
Registered: ‎02-07-2002

Re: experience in standard gcc compiler for SS4

Then I expect you want to use Zigbee or Thread and the answer is no AFAIK.

Posts: 11
Registered: ‎01-20-2017

Re: experience in standard gcc compiler for SS4

yes I want to use Thread with this...

Posts: 263
Registered: ‎12-05-2016

Re: experience in standard gcc compiler for SS4

Hi @Hobbit23,

 

@vanmierlo is correct, The Zigbee and Thread stacks currently only support the IAR compiler.  With the latest release the Bluetooth stack (v2.3.0.0) has added beta support for the gcc compiler.

 

Thank you,

jpitt