Reply
Posts: 261
Registered: ‎09-07-2012

energyAware Commander 2.83

Hi,

 

Here's a new beta release of energyAware Commander.

 

Zero Gecko unlock also requires a new kit firmware, to be released in beta soon.

 

Changes since 2.82:

* Added support for Zero Gecko unlock.
* Added support for Linux x86_64.
* Fixed issue with connection failed when starting from command line repeatedly.
* Fixed firmware upgrade on Mac OS X and Linux x86_64.

 

Downloads:

Windows

Mac

Linux (i386)

Linux (x86_64)

Posts: 261
Registered: ‎09-07-2012

Re: energyAware Commander 2.83

A firmware package which supports unlocking ZG devices is now available here: http://community.silabs.com/t5/Tools-Beta-Releases/STK3200-STK3600-STK3700-STK3800-Firmware-0-9-14-b...

Posts: 21
Registered: ‎01-22-2013

Re: energyAware Commander 2.83

[ Edited ]

EDIT:
Nevermind this post (it was just './eACommander --help' of course...)

---

Hi. Where can I find documentation for the command line options of (this version of) eACommander? (I'm trying to flash to one of several connected kits using the command line)

 

Thanks Robot Happy

-Erik

Highlighted
Posts: 7
Registered: ‎05-15-2013

Re: energyAware Commander 2.83

Pssst, link is broken Robot Sad