Using EFM8 with Keil RTX51 TINY in Simplicity Studio

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> Jiehui on ‎03-13-2017 11:45 AM

Question

Using Simplicity Studio V4, there is an RTX51.LIB error after building after adding Keil RTX51 Tiny code into my 8051 project.

RTX51_error.png

How can I fix this problem?

Answer

The Keil RTX51 Tiny Real-Time kernel is included in the PK51 Professional Developer's Kit.

 

Using the LX51 linker, add the RTX51TINY directive to specify that the project being linked is a real-time application that uses the RTX51 Tiny Real-Time Operating System. This can be done in the Properties of the current project in Simplicity IDE: Settings > Keil 8051 Linker > Miscellaneous > Additional Flags. Finally re-build the project again.

 

LX51_RTX51TINY.png

 

An unlimited Keil PK51 license is provided for 8-bit Silicon Labs MCUs. Register your product and received the key to unlock your PK51 tools from Simplicity Studio > Help > Licensing or from here.