Reply
Posts: 46
Registered: ‎10-17-2016

Trojan-DropperGB.17644 found in .jar file

I've just had the following AV alert!

StudioAV.png

Posts: 523
Registered: ‎12-05-2016

Re: Trojan-DropperGB.17644 found in .jar file

Hi @digisolve,

 

Was the virus detected during a Simplicity Studio update or when did it occur?  I have seen false positive malware detection reported on the .exe files in adapter packs, but this is different than that.  I will also respond to the support case that was created for this issue.  If possible please use one of the online scanner tools available from different anti-virus companies to confirm it the files are really infected or not.  This is the first report I'm seeing of this type of infection, so I do thing it is an isolated event.  The screenshot you uploaded shows two versions of the same file being infected.  I have scanned several recent installations of that file and I haven't found any that were infected.

 

Thank you,

jpitt