Reply
Posts: 54
Registered: ‎09-06-2017
Accepted Solution

Simplicity studio prompts to update every run

Every time I run simplicity studio it says there are updates available. If I review updates there are none. Is there anything I can do?

Highlighted
Posts: 523
Registered: ‎12-05-2016

Re: Simplicity studio prompts to update every run

Hi @nickb,

 

In the Package Manager (updater) is the SDKs tab red with a number on it?  If so select that tab and then set the Version filter to "Installed" and check for any packages that have "Update" available for the status.  If there is one and you wish to update that SDK (and no imminent releases that depend on the existing version) then go ahead and update it.

 

Thank you,

jpitt