Simplicity IDE

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> Alan_S on ‎12-02-2016 10:28 AM

Question

Is it possible to change a project's device after it is created?

Answer

Yes, you can change the device that the project is configured for by opening the Properties of the project you want to change. Under C/C++ Build -> Board/Part/SDK, there is an option to change the Boards and then Part fields for that particular project.