Reply
Highlighted
Posts: 4
Registered: ‎07-07-2014
Accepted Solution

Simplicity Configurator code for EFM32 does not compile

Hi everyone,

I'm trying to set up a basic project using I2C.

To save some time looking up the proper pin and port configurations I thought of using the configurator.

Now, without having anything enabled in the configurator yet, I only included the "enter_DefaultMode_from_RESET"-function in my main(), the compiler throws an error:

Debug/../src/InitDevice.c:41: undefined reference to `CMU_ClockSelectSet'

 

This happens despite the fact that "em_cmu.h" is included in the InitDevice.c

An additional "undefined reference"-error shows up when I try to include the I2C part.

I've looked through AN0823 but it didn't reveal anything helpful for this issue to me.

Any help how to resolve this is appreciated!

 

Regards Chris

Posts: 2,875
Registered: ‎02-07-2002

Re: Simplicity Configurator code for EFM32 does not compile

I suspect this is a linker error instead of a compiler error. Have you included the source file that implements CMU_ClockSelectSet() in your project?

Posts: 1
Registered: ‎03-18-2015

Re: Simplicity Configurator code for EFM32 does not compile

Hi, You wrote: "I only included the "enter_DefaultMode_from_RESET"-function". Did You included other functions, that are called from function "enter_DefaultMode_from_RESET"-function"?

I suggest include whole file and header file InitDevice.c and InitDevice.h

Be aware from errors in Configurator. Some Clock initializations are missing in functions.

Martin

Posts: 4
Registered: ‎07-07-2014

Re: Simplicity Configurator code for EFM32 does not compile

You're right, that was the issue.

Even though I don't understand, why it is neccessary to include the source files manually though.

If I use a configurator I'd expect it to take care of this, or at least show a message that it doesn't and I need to manually (!) copy (or copy by reference) the source files into the project each time!

 

Thanks for your help :-)