Reply
Posts: 2,968
Registered: ‎02-07-2002
Accepted Solution

STK/WSTK Debug Adapter

Since there is no Hardware Tools subforum under "Hardware and Software Tools" I post this in "Simplicity Studio and Software".

 

I would like to know if the schematics and BOM of the STK/WSTK Debug Adapter a.k.a. BRD8010A are available somewhere? There is AN958, but it doesn't show exactly what is on the board. I like the idea of the Simplicity Mini connector, but I find the thing too small. I would like my colleagues to be able to create a different adapter that more easily connects to our boards.

Posts: 194
Registered: ‎08-19-2015

Re: STK/WSTK Debug Adapter

Hi @vanmierlo,

 

Thank you for contacting Silicon Labs regarding the STK/WSTK Debug Adapter board (BRD8010A).  I have attached the schematic pdf, BOM, and assembly drawing to this forum post for your reference.  I hope this helps, and please let me know if you have any further questions.

 

Regards,

Mitch

MCU Applications Engineer

Posts: 2,968
Registered: ‎02-07-2002

Re: STK/WSTK Debug Adapter

Thank you very much. This is exactly what I needed.

Highlighted
Posts: 194
Registered: ‎08-19-2015

Re: STK/WSTK Debug Adapter

You're welcome and no problem!

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Star</font></font> </a> may
Posts: 4
Registered: ‎06-20-2017

Re: STK/WSTK Debug Adapter

buen dia me gustaria saber si el debuger P&E micro es compatible con silmplicity studioo

Posts: 1,955
Registered: ‎10-14-2014

Re: STK/WSTK Debug Adapter

translate to English
----------------------------------------------------------------
Good day I would like to know if the debugger P & E micro is compatible with silmplicity studio.
----------------------------------------------------------------

https://www.pemicro.com/
WeiguoLu