Reply
Posts: 7
Registered: ‎07-13-2014
Accepted Solution

Problem with save and restore APSR

I have some problem for asm-program. I need to save and restore
carry or borrow flag in Application Program Status Register (APSR)
in my program for subtract.very long degits. I used next commands:

        .thumb_func
        .type   LFIX_sub, %function
        .global LFIX_sub
LFIX_sub:
        .fnstart
        .cantunwind

         push    {r3-r6}
         ldr     r3,[r0],#4
         ldr     r4,[r1],#4
         subs    r3,r4     
         mrs     r6,APSR   // save MCU flags
         str     r3,[r2],#4
         mov     r5,#count
.L1_sub:
         ldr     r3,[r0],#4
         ldr     r4,[r1],#4
         msr     APSR, r6  // restore MCU flags
         sbcs    r3,r4     
         mrs     r6,psr    
         str     r3,[r2],#4
         subs    r5,#0x1   
         bgt.N   .L1_sub   
         pop     {r3-r6}
         BX      LR        

        .fnend
        .size   LFIX_sub, .-LFIX_sub

    I have error for command "msr APSR, r6":
<writing to APSR without specifying a bitmask is deprecated>

   I look all examples and manuals carefully . I can not find syntax to
write bitmask in my command. How I must write my command without mistake.

Posts: 433
Registered: ‎12-05-2016

Re: Problem with save and restore APSR

[ Edited ]

Hi @Kalaxara,

 

Please try changing the command from

msr     APSR, r6  // restore MCU flags

 

to 

msr     APSR_nzcvq, r6  // restore MCU flags

 

Apparently the bitmask that is desired consists of specifying which of the status bits are to be written back to the APSR register.

 

Thank you,

jpitt

Highlighted
Posts: 7
Registered: ‎07-13-2014

Re: Problem with save and restore APSR

It's really help me. Мany thanks.