Launch Simplicity Studio using a specified workspace

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> ChrisM on ‎11-04-2016 02:22 PM

Question

How do I start Simplicity Studio using a specified workspace?

Answer

Use the -data command line flag to launch a Studio session with the specified workspace path.

 

For example, to launch Studio v4 using the default installation folder using a workspace located at C:\Users\<user>\SimplicityStudio\v4_test, execute the following command:

 

C:\SiliconLabs\SimplicityStudio\v4\studio.exe -data "C:\Users\<user>\SimplicityStudio\v4_test"  

Note: Windows paths with spaces must be enclosed in double quotes (").