Reply
Posts: 76
Registered: ‎11-03-2016
Accepted Solution

I can't install Simplicity Studio in Win7 (error code -5006 : 0x80070020)

I downloaded the SE4 installer but when trying to execute it, it generates the following error:

 

SE4Error.png

 

What does it mean?

 

It is complaining about closing other applications and verify any previous setups, but I'm running it from a fresh reboot.

Posts: 582
Registered: ‎12-05-2016

Re: I can't install Simplicity Studio in Win7 (error code -5006 : 0x80070020)

Hi @mmalagon,

 

That error is indicating a resource is being held by another process.  Can you start the Windows task manager to see if any other updates are going on or another process that might be interfering? (Possibly a Windows update or something like that).  Is it possible the antivirus program is preventing the installation? Also since this is a server are there other users that are automatically logged on that might somehow be interfering with the installation?

 

Thank you,

jpitt

Posts: 76
Registered: ‎11-03-2016

Re: I can't install Simplicity Studio in Win7 (error code -5006 : 0x80070020)

@jpitt after reading your response, I decided to run the installation again and it worked. You are right,  maybe on that occasion, some windows stuff was happening in the background.

 

Anyways, now I was able to install SS4

 

Thanks for helping!