Reply
Posts: 3,100
Registered: ‎02-07-2002

How to clear the Problems log?

Hello,

 

I've created an EFR32 RAIL project from the Simple Rail with Hal template. When building I get the following warning:

Invalid project path: Include path not found
C:\...\SiliconLabs\SimplicityStudio\v4\developer\sdks\gecko_sdk_suite\v1.1\
platform\Device\SiliconLabs-Restricted\EFR32FG1V\Include

Of course I have no SiliconLabs-Restricted directory on my system. And thus I removed it from the project settings.

 

Now the issue is that I cannot get rid of the warning in the Problems View. I've already freshened and rebuilt the C/C++ Index, but it doesn't help. Restarting Studio also has no effect. How am I supposed to get rid of it?

 

Maarten

Highlighted
Posts: 523
Registered: ‎12-05-2016

Re: How to clear the Problems log?

Hi @vanmierlo,

 

That is an annoying warning, I'm not sure why that include path is included in the project.  I was able to remove the warning by removing that path from the project properties GNU ARM C Compiler -> Includes and hit "Apply" and then also remove it from the GNU ARM Assembler -> General tab Include paths and also hitting "Apply" and then 'OK'.  If I just hit 'OK' it seemed like it got added back to one or the other places.

 

I hope that resolves the issue for you.

 

Thank you,

jpitt