Cloning a Git repository on Simplicity Studio V3

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Ninja Employee</font></font> </a> marao on ‎09-21-2016 11:50 AM

Once you have Git set up on Simplicity Studio V3 (see KB article - Source Control with Studio V3), you can clone a Git repository using the following steps:

 

1. In the Git perspective, click Clone a Git repository

 

Egitv3_7.png

 

2. Enter the URL

 

Egitv3_8.png

 

3. The other fields will auto-populate. So hit Next and finally, Finish

 

Egitv3_9.png

 

 4. Once the repository is cloned, right click the repo and select Import Projects

 

Egitv3_10.png

 

5. Hit Next >> Finish, and all the projects should be imported

 

Egitv3_11.png

 

6. All the projects are now located in the IDE workspace and are available to build. Switch perspective back to the Simplicity perspective to see all the projects in the workspace. 

 

Egitv3_12.png

 

7. Change and build projects here. You have successfully cloned your Git workspace into Simplicity Studio!

 

Egitv3_13.png