Changing editor font and size in Studio

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> ChrisM on ‎09-12-2016 06:22 PM

Question

How do I change the font and font size in Studio?

Answer

Change the font by performing the following steps:

  1. Open Simplicity IDE
  2. Press Ctrl+3
  3. Search for "font"
  4. Select "Colors and Fonts"
  5. Many fonts inherit from the default font specified under the "Basic" category
  6. To change text font commonly used in editors, select "Basic"->"Text Font"
    colors_and_fonts_basic_text_font.png
  7. Click "Edit"
  8. Change the font, font style, and size as desired and click "OK"
    colors_and_fonts_basic_text_font_edit.png
  9. Click "OK" to apply the new font settings
    colors_and_fonts_basic_text_font_editor.png
  10. Reset a selected font back to default settings using the "Reset" button in the "Colors and Fonts" dialog