Change variable/expression number format in Simplicity Studio debugger

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> ChrisM on ‎08-23-2016 07:40 PM

Question

How do I display values in Simplicity Studio debugger as hex?

Answer

Most views that display values in the debug perspective can format values in different ways.

 

To change the number format, perform the following steps:

1. Start a debug session, switching automatically to the debug perspective.

2. Select the Variables or Expressions view.

3. Click the down arrow button in the top right corner of the view.

4. Select Hex from the Number Format menu.

number_format_hex.png