Reply
Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Ninja</font></font> </a> tj
Posts: 54
Registered: ‎07-04-2016

Can't connect to incompatible device

After last Simplicity Studio update I can't connect to incompatible device. I have own board with EFR32MG1P232F256GM32

When debug start I got warning, click Yes and got error " The given part number EFR32MG1P232F256GM32 does not match the detected device EFR32MG1P232F256GM48".

 

Before last update this operation worked correctly.

I can't change to proper device in HW configurator, becouse I got Internal Error:  java.lang.NullPointerException

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Ninja</font></font> </a> tj
Posts: 54
Registered: ‎07-04-2016

Re: Can't connect to incompatible device

Here is screenshot

Posts: 441
Registered: ‎12-05-2016

Re: Can't connect to incompatible device

Hi @tj,

 

I am seeing similar issues with the latest Simplicity Studio update. I am investigating it and I will let you know what I find out.

 

Thank you,

jpitt

Posts: 441
Registered: ‎12-05-2016

Re: Can't connect to incompatible device

Hi @tj,

 

We found some problems with some of the efr32 asset files.  These were corrected and published last night.  Please do a studio update again, there should be 5 asset updates for the efr32 devices.

 

After updating, please let me know if this issue still exists.

 

Thank you,

jpitt

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Ninja</font></font> </a> tj
Posts: 54
Registered: ‎07-04-2016

Re: Can't connect to incompatible device

I don't see updates. In package manager I have messsage: "No Product Updates packages available"

Posts: 441
Registered: ‎12-05-2016

Re: Can't connect to incompatible device

Hi @tj,

 

Please check for updates periodically.  Silicon Labs uses a content delivery service to distribute the download assets across the world and I have heard of others that didn't see an update for a few days.  I will investigate the timing of when updates are available, but it would be beneficial to hear when you see the update.

 

Thank you,

jpitt

Posts: 1
Registered: ‎02-18-2017

Re: Can't connect to incompatible device

I have the exact same problem with EFM32G210F128.  Any chance there is a solution for this too?

Posts: 441
Registered: ‎12-05-2016

Re: Can't connect to incompatible device

Hi @kevinko,

 

The screenshot is showing the project was built for device efm32lg990f256, but the device connected to Simplicity Studio is an EFM32G210F128.  What device is shown in the "Devices" window?  Expanding the J-Link Silicon Labs line in the "Devices" window and the lines under it until the device is shown.  If the Devices window shows efm32lg990f256, but the actual device is the EFM32G210F128, then the detected device might be overridden in the configuration for this WSTK (or J-Link serial number).  If that is the case then right clicking the top level "J-Link Silicon Labs" line and choosing "Device configuration..." will open a dialog box.  Click the "Device hardware" tab.  If the part listed under Target part is efm32lg990f256, then enter "None" where it says "Search" below Target part: and click OK to clear the override and revert back to the detected part.  Programming and debugging can then happen on the detected part.

 

I hope this is helpful information.

 

Thank you,

jpitt

 

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Ninja</font></font> </a> tj
Posts: 54
Registered: ‎07-04-2016

Re: Can't connect to incompatible device

Hi @jpitt

 

I have checked updates after 9 days and I see updates for Commander only.

 

Posts: 441
Registered: ‎12-05-2016

Re: Can't connect to incompatible device

Hi @tj,

 

I should have asked how you are connecting to the board?  Do you have a WSTK that is set to Debug OUT mode and then a cable running from the debug port to your custom board or something else?  If so please make sure the Debug Mode of the WSTK is still set to OUT.  If the connection to the board is some other way please provide the details of how it is connected.

 

Thank you,

jpitt

 

 

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Ninja</font></font> </a> tj
Posts: 54
Registered: ‎07-04-2016

Re: Can't connect to incompatible device

Today I have installed 63 updates in SimplicityStudio, but problem with incompatibile device still exist.

I can't change to proper device in HW configurator, becouse I got Internal Error: java.lang.NullPointerException

 

I still have to use very old SimplicityStudio version with security issues....Smiley Sad

 

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Ninja</font></font> </a> tj
Posts: 54
Registered: ‎07-04-2016

Re: Can't connect to incompatible device

Regarding about connection, I have my custom board connected as WSTK, I don't use debug out connector.

Posts: 441
Registered: ‎12-05-2016

Re: Can't connect to incompatible device

 
Posts: 441
Registered: ‎12-05-2016

Re: Can't connect to incompatible device

Hi @tj,

 

Are you saying your custom board is connected directly to the PC without using a Silicon Labs WSTK?  If so are you using a J-Link pro or other Segger device or is it connected via an ethernet port or is there a J-Link device on your custom board? If you run the Device inspector for Exx32 can you paste the output to this Forum thread? ([Window] > [Preferences] > [Simplicity Studio] > [Adapter Packs] > [Device inspector for Exx32 and EFM8 hardware [built-in]] and then select the last entry "inspect: $(inspect_emdll) -slist [ -sn ${sn}], batch" and click Bare run, then leave the sn box blank and click [OK].

 

Thank you,

jpitt

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Ninja</font></font> </a> tj
Posts: 54
Registered: ‎07-04-2016

Re: Can't connect to incompatible device

Hi @jpitt

 

WSTK - Do you mean PCB4001A or BRD4151A ?

 

I have two hw setup, with

- PCB4001A + coustom board connected as daughter board

- J-Link base + coustom board

 

Here is the log:

Executing: C:\prg\SiliconLabs\SimplicityStudio\v4\developer\adapter_packs\inspect_emdll\inspect_emdll.exe
==================================
# Simplicity Studio device detection

deviceCount=1

device(440053578) {
  serialNumber=440053578
Connecting to device with serial number 440053578 .. ok.
EMDLL version: 0.13.4b233
J-Link DLL Version: 6.14`
  AdapterType=JLink
  adapterLabel=J-Link Silicon Labs
  adapterId=4001A
  adapterName=BRD4001A Rev. A01
  adapterDescription=Wireless Starter Kit Mainboard
  adapterRevision=A01
  adapterSerialNumber=153108406
  adapterDate=0/0/0
  adapterFirmware=0v15p3b562
  adapterFpga=15v15p255b65535
  adapterInBootloader=no
  supportedDebugModes=OFF,MCU,IN,OUT
  debugMode=MCU
  inferPart=yes
  supportsAEM=yes
  supportsVCom=yes
  supportsEmucom=yes
  supportsIP=yes
  boardCount=1
  boardId[0]=4001A
  boardName[0]=BRD4001A Rev. A01
  boardDescription[0]=Wireless Starter Kit Mainboard
  boardRevision[0]=A01
  boardSerial[0]=153108406
  boardDate[0]=2015/10/30
  inferPart[0]=yes
}


==================================
with J-Link base

Executing: C:\prg\SiliconLabs\SimplicityStudio\v4\developer\adapter_packs\inspect_emdll\inspect_emdll.exe
==================================
# Simplicity Studio device detection

deviceCount=1

device(59305138) {
  serialNumber=59305138
Connecting to device with serial number 59305138 .. ok.
EMDLL version: 0.13.4b233
J-Link DLL Version: 6.14`
  AdapterType=JLink
  adapterLabel=J-Link
inspect_emdll [ERROR: EMDLL error -501: GetDebugMode
]
inspect_emdll [ERROR: EMDLL error -501: AdapterInfoGet
]
  boardCount=1
  boardId[0]=36U
  boardName[0]=¸˛ž
  boardDescription[0]=
  boardRevision[0]=K158
  boardSerial[0]=1044442112
  boardDate[0]=65027/65535/56063
  inferPart[0]=no
}


==================================