Reply
Posts: 9
Registered: ‎08-23-2017
Accepted Solution

Building micriumos_wifi_whiteboard example source, won't build

Hi,

It's me again trying to build the micrium_wifi_whiteboard example application with Studio v4 and 32bit MCU SDK v5.2.2

It won't build whether I create the project from the Launcher software example list, or I create it by manually creating the project.  I am attaching the project file and the console output in a word file.

Help please.

Dan

 

 

Posts: 2,326
Registered: ‎10-14-2014

Re: Building micriumos_wifi_whiteboard example source, won't build

[ Edited ]

folder.pngIt looks like the folder structure has some problem.

Do you see the util/micrium/Micrium_OS folder on you simplicity studio.

 

WeiguoLu
Posts: 2,326
Registered: ‎10-14-2014

Re: Building micriumos_wifi_whiteboard example source, won't build

Try to update the simplicity studio to add the micrium 5 (you should see it in SDK tab).

Then you could see a new folder create under:

C:\SiliconLabs\SimplicityStudio\v4_3\developer\sdks\gecko_sdk_suite\v1.1\util\micrium

Then the build should pass.

Good luck!

WeiguoLu
Posts: 9
Registered: ‎08-23-2017

Re: Building micriumos_wifi_whiteboard example source, won't build

Yes that worked.  I had to manually load the Micrium SDK.