Reply
Posts: 10
Registered: ‎10-11-2017

Bootload Run Command failure

Hello,

 

I have purchased a ToolStick with a C8051F330 daughter card.  I have installed Simplicity Studio V4 in Linux.

 

So far, I have been unable to communicate with the device.  When I try to run or debug software, there is an error message: Bootloader returned failure response.

 

The device manager identifies my board as TOOLSTICK330DC.

 

When I try to run flash8051 directly, e.g. "flash8051 -sn TS004A9750 -checkunlock" I get

 

OSX firmware update in progress.Bootload Run Command failure: status:00, FWresponse:00.
Firmware execution error: status:00.
Incorrect Firmware version download!Communication could not be established with the specified adapter.
Please confirm the current adapter selection and cable connection.flash8051 [ERROR: Bootloader returned failure response.]

Posts: 10
Registered: ‎10-11-2017

Re: Bootload Run Command failure

I see this in the system log when I connect the ToolStick:

 

usb 1-2: New USB device found, idVendor=10c4, idProduct=8253
usb 1-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
usb 1-2: Product: ToolStick
usb 1-2: Manufacturer: Silicon Laboratories
usb 1-2: SerialNumber: TS004A9750

hid-generic 0003:10C4:8253.0004: usb_submit_urb(ctrl) failed: -1
hid-generic 0003:10C4:8253.0004: timeout initializing reports
hid-generic 0003:10C4:8253.0004: hiddev0,hidraw0: USB HID v1.11 Device [Silicon Laboratories ToolStick] on usb-0000:00:14.0-2/input0

 

Posts: 10
Registered: ‎10-11-2017

Re: Bootload Run Command failure

Maybe this can help.  I'll try it later.

 

https://bbs.archlinux.org/viewtopic.php?id=192969