Reply
Posts: 2
Registered: ‎03-06-2017

use BTLE-Stack and Rail on EFR32FG1P133F256GM48

Hi,

 

is it possible to install BTLE-Stack and Rail on EFR32FG1P133F256GM48. The device should run with SUB GHz proprietary protocol, but configurations should be done by BTLE.
If not, will it be possible in future or by other devices?

Thanks

Posts: 36
Registered: ‎05-08-2015

Re: use BTLE-Stack and Rail on EFR32FG1P133F256GM48

Hi,

Please check the Wireless Selector Guide at our website. What you are looking for is the P line of the EFR32BG family (not FG).

 

Regards,

Jose

Posts: 2
Registered: ‎03-06-2017

Re: use BTLE-Stack and Rail on EFR32FG1P133F256GM48

Hi,

 

thanks for the answer!

I need the EFR32FG for the main function (Sub GHz 169 MHz) of our device. So I can not use the EFR32BG family. The idea is to use BLE only for configuration in a special device mode.
I think  the EFR32FG1P133F256GM48 can do the modulation and the frequency hopping which is need for BLE.  So I am wondering, if it is possible make the  BLE stack in EFR32FG1P133F256GM4 run.

Regards
Klaus