Reply
Posts: 2
Registered: ‎09-04-2017

radio-configurator_ SLWSTK6240A.isc can't be opened

Hello, I just make my custom wireless board with EZR32HG220 and most of the examples are successfully running on the board, now I use two boards to check the link functionality with direct TX and direct RX, according to AN1004-RF-evaluation-EZR32, the radio configurator is used to configure and modify the radio, but I can not open this plugin, anybody pls tell me the reason or I missed some information?

 

Posts: 193
Registered: ‎06-11-2015

Re: radio-configurator_ SLWSTK6240A.isc can't be opened

It does work for me.

Please make sure you're using an up to date Studio and the latest Gecko SDK suite. If it still doesn't work, open the error log window (window/show view/other/error log), and see what it says when you're trying to open it.

 

Andras

Posts: 2
Registered: ‎09-04-2017

Re: radio-configurator_ SLWSTK6240A.isc can't be opened

Hi, Thanks guy!

The problem appeared at MAC os, after I changed a windows version, the .isc file could be opened and configured. I will check the log file latter.