Reply
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Star</font></font> </a> aku
Posts: 2
Registered: ‎09-23-2015

Unable to connect to energy harvesting ref board (SI1012)

Hello.

I can see the toolstick in the IDE config menu. Upon "connect" the IDE tells me firmware needs to be updated. After some activity (downloadinf FW) it fails with "incorrect firmware version".

The board runs OK with the built-in wireless sensing application when using USB power. The battery appeas to be dead, however.

Any ideas?

Highlighted
Posts: 1
Registered: ‎09-25-2015

Re: Unable to connect to energy harvesting ref board (SI1012)

I met the same problem