Reply
Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Star</font></font> </a> woo
Posts: 1
Registered: ‎10-12-2017

RAIL 4-GFSK configuration

Hi, all I am using EFR32FG1P133F256GM48 (4250A EVM) and want to use 4-GFSK 200kbps. I confirmed that 2-GFSK 100kbps, then trying to configure 4-GFSK 200kbps by using 2-GFSK 100kbps configuration. Becasue Simplify Studio only provide 2-GFSK configuration files(.isc), so it's difficult to configure 4-GFSK. Please help me to solve this problem.
Posts: 101
Registered: ‎12-02-2016

Re: RAIL 4-GFSK configuration

Hi,

 

Which version of SSv4/Radio configurator do you use?

I've checked the tools with the latest version,  FSK4 is there. 

Attachment is a screenshot about the radio configurator.

 

If the SSv4/Radio configurator is not the latest version, please upgrade first.

 

Regards,

Yongsheng