Reply
Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Genius</font></font> </a> AV
Posts: 38
Registered: ‎12-15-2015
Accepted Solution

Note about the use of a Si4464

In Table 3 of the si4464/63/61/60 devices it is told (see page 7, Note 2) that, if possible, the Si4463/61/60 should be used instead of the Si4464.

 

What is the reason for this recommendation?

 

Thank you very much and best regards,

 

Alberto

 

 

 

 

Posts: 132
Registered: ‎01-06-2015

Re: Note about the use of a Si4464

Hi Alberto,

 

The main reason for this recommendation is that the Si4464 is dedicated for +20dBm applications, while if you choose one radio from Si4460/61/63, you can select the one that fits best for your power requirements. For instance, if you need only +10dBm conducted power, you should go with Si4460 to have optimal current consumption for that power. By using Si4464 for +10dBm would generate extra current consumption, since it is not designed for that power range.

 

Also, Si4460/61/63 exist in revC version, while Si4464 has revB radio inside, but that is just an additional note, and not an explanation for the datasheet recommendation.

 

Daniel

<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Genius</font></font> </a> AV
Posts: 38
Registered: ‎12-15-2015

Re: Note about the use of a Si4464

Thank you very much, Daniel!

 

Alberto