Reply
Posts: 2
Registered: ‎08-22-2017

How to increase the maximum number of si4432 clients to connect to a single si4432 server?

Hi,

I am working on a si4432 related project where there is a Client - server communication.What is the maximum number of clients that can be connected to a single si4432 server?And what is the procedure to increase the maximum number of clients that can be connected to a single server as I am going to connect 900 si4432 clients to a single server? 

Highlighted
Posts: 38
Registered: ‎02-18-2014

Re: How to increase the maximum number of si4432 clients to connect to a single si4432 server?

rakesh4683,

 

The maximum number of connected clients depends on the protocol used. What kind of stack are you using?

 

Imre

Posts: 2
Registered: ‎08-22-2017

Re: How to increase the maximum number of si4432 clients to connect to a single si4432 server?

You mean protocol for Si4432? I think Si4432 do not have any protocol.

Actually I am using Si4432 for receiving and transmitting some data.I am using a single Si4432 as receiver and above 900 Si4432s as clients.I am modifying the registers 3F-42 as mentioned in the datasheet.After modification there is no communication.

Can you tell whether Si4432 uses 4 byte addressing?