Reply
Posts: 7
Registered: ‎04-05-2015

How can i make header file on WDS?

Dear Sir,

 

I used SI4463, so I want to change frequency, baudrate etc...

I found following data on other person of  source code.

But I can't make same heder file on WDS 3.2 version.

How can i make this?

 

#define CENTER_FREQ 447867500
#define XTAL_FREQ 30000000
#define CHANNEL_SPACING 250000
#define CHANNEL_NUMBER 0
#define XTAL_CAP_BANK 0x52
#define MODULATION_TYPE "2FSK"
#define MODULATION_TYPE_VALUE 2
#define MANCHESTER_CODE "Off"
#define MANCHESTER_CODE_VALUE 0
#define DEVIATION 3500
#define DATA_RATE 1200
#define ANTENNA_DIVERSITY "Disabled"
#define ANTENNA_DIVERSITY_VALUE 0


// # WB filter 3 (BW = 46.31 kHz); NB-filter 3 (BW = 46.31 kHz)

// Modulation index: 7


// # Warning:
// # Modulation index is >=2, async demodulator is used

// Calculator svn revision 6181

// EZRadio PRO2 modem calculator output header file modem_params.h

// RF frequency is 447.99 MHz
// Mod type: 2FSK, DataRate: 1.00 ksps; FreqDev: 3.50 kHz; RX BW: 43.00 kHz

// all for TX in this section:
// DataRate: 3 API bytes; NCOMODulus: 4 bytes; FreqDev: 3 bytes, for TX
#define MODEM_DATA_RATE_2_14 0x11, 0x20, 0x0A, 0x03, 0x00, 0x03, 0xE8, 0x00, 0x2D, 0xC6, 0xC0, 0x00, 0x00, 0xF5
#define MODEM_TX_RAMP_DELAY_5 0x11, 0x20, 0x01, 0x18, 0x01
// PA ramp time control: 1 byte
#define PA_TC_5 0x11, 0x22, 0x01, 0x03, 0x1C


// all for general parameters in both TRX
#define MODEM_MOD_TYPE_7 0x11, 0x20, 0x03, 0x00, 0x02, 0x00, 0x07
#define MODEM_CLKGEN_BAND_5 0x11, 0x20, 0x01, 0x51, 0x0A
// SYNTH CONTROL GROUP: 7 API bytes, for both TRX
#define SYNTH_PFDCP_CPFF_11 0x11, 0x23, 0x07, 0x00, 0x2C, 0x0E, 0x0B, 0x04, 0x0C, 0x73, 0x03
// FREQ CONTROL GROUP: 8 API bytes, TRX
#define FREQ_CONTROL_INTE_12 0x11, 0x40, 0x08, 0x00, 0x3A, 0x0D, 0xDA, 0x74, 0x00, 0x00, 0x20, 0xFE

Posts: 245
Registered: ‎12-10-2013

Re: How can i make header file on WDS?

The code you referred to is an old example code for si446x.

 

Please use WDS to generate the latest demo code and the header file(for API setting). Please don't used the old version of WDS.

 

Thanks,

Juanyong

Posts: 7
Registered: ‎04-05-2015

Re: How can i make header file on WDS?

Dear Sir,

 

Which version of WDS?

If you know, pls say to me.

I will request old version to SILAB for my project.

 

Thanks Regards

Posts: 245
Registered: ‎12-10-2013

Re: How can i make header file on WDS?

The latest WDS is version 3.2.11.0, which can be downloaded from: http://www.silabs.com/support/resources.p-wireless_proprietary_ezradiopro_si4463.page=1

 

Silabs updated the WDS in order to get optimal performance, fix bugs, and upgrade to support latest version chip(for example from B0-->B1-->C2 for si446x). You shouldn't use that version WDS(which has the header file format you mentioned).

 

 

Thanks,

Juanyong