Reply
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Star</font></font> </a> AM1
Posts: 2
Registered: ‎04-07-2017

EZR32LG vs Si1060 - RF core

Hi,

 

Does EZR32LG have the same RF core as Si1060? Can they be initialized and used 100% the same or there are differences and where I can find these differences?

 

Thanks

Posts: 44
Registered: ‎05-08-2015

Re: EZR32LG vs Si1060 - RF core

Hi,

The correct answer is Almost. Both wireless MCUs use the Si4463 radio, but the Si1060 has rev B, the EZR32LG has the newer revision C. Differences can be found in application note AN897: 

http://www.silabs.com/documents/public/application-notes/AN897.pdf

Regards,

Jose

Highlighted
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Star</font></font> </a> AM1
Posts: 2
Registered: ‎04-07-2017

Re: EZR32LG vs Si1060 - RF core

That was helpful. Thank you