Reply
Highlighted
Posts: 4
Registered: ‎03-20-2017

EZR32LG Fail running Simple TRx example

Hi,

 

I'm running Simple TRx example (without changes) under EZR32LG, but some problems are happening.

 

First:

When Board 1 and 2 are changing packets, apparently the sequencwe is broken, Board 1 sends the correct sequence but Board 2 receives an old packet. (attached file 1)

 

Second:

Incorrect received data as showed in attached file 2. I was hopping, in that case, a CRC error during transmission.

 

 

Best regards,

Denis

Posts: 101
Registered: ‎12-02-2016

Re: EZR32LG Fail running Simple TRx example

Hi Denis,

First:   I have checked, the program run normally, and couldn't reproduce your question. I created the project based on Gecko SDK v5.0.0.

Second:  Which demo code did you test about frequency hopping?   The simple TRX project we provide doesn't contain frequecy hopping.

 

Posts: 4
Registered: ‎03-20-2017

Re: EZR32LG Fail running Simple TRx example

Hi Yongsheng,

 

I'm using Gecko SDK v5.0.0 too.

When I sad hopping the correct was hoping or expected.

 

Sorry about the long time, I was out.

 

Posts: 101
Registered: ‎12-02-2016

Re: EZR32LG Fail running Simple TRx example

Hi Denis,
When you read the whole demo code, you'll find if there's a crc error, "-->Pkt  RX: CRC Error" will be printed on the LCD screen.
But, the screenshot you sent is not, it seems the received packet passed with crc checking.

SO, I think there should be some problems about your code with the board.
What's board do you use for testing?  Is it a standard WSTK from silabs?
Could you send your whole source project to me for a further analysis?

Regards,
Yongsheng