Reply
Highlighted
Posts: 1
Registered: ‎10-11-2016

EFR32MG Mighty Gecko/Connect stack frequency hopping?

[ Edited ]

Hi,

 

Does the Mighty Gecko (EFR32MG1P233F256GM48) running the Connect stack support frequency hopping? If yes, is there an example application?

 

I have the Mighty Gecko Development kit plus three of the above modules (BRD4150B). I tried the sink/sensor application and saw no frequency hopping. I tried both "US/FCC 902MHz-928MHz" and "DSSS 100Kbps" configurations.

 

Thanks.

Posts: 198
Registered: ‎06-11-2015

Re: EFR32MG Mighty Gecko/Connect stack frequency hopping?

This is under development, if everything goes well, we will release it in the end of this year.

 

Regards,

Andras

Posts: 76
Registered: ‎11-03-2016

Re: EFR32MG Mighty Gecko/Connect stack frequency hopping?

@andrasbiro so the Mighty Gecko will support frequency hopping at the end of 2016?

 

Because I'm about to start a project that absolutely needs frequency hopping and this would be really helpful!

Posts: 198
Registered: ‎06-11-2015

Re: EFR32MG Mighty Gecko/Connect stack frequency hopping?

In connect, yes. A decision was made that RAIL shouldn't support frequency hopping, it should be in an upper layer (but it's certainly possible from the application).