Reply
Posts: 1
Registered: ‎10-05-2017

EFR32FG Wireless communication

Hi

 

Im doing a school project about wireless communication between two MCUs.

My goal with the project is to send a string of data between two MCUs every second.

 

Is it possible to import a code that handles the sending/receiving of the string somewhere in the Rx/Tx part of the main.c file?

 

Any inputs would be very helpful!

 

Have a nice day.

 

Posts: 47
Registered: ‎02-18-2014

Re: EFR32FG Wireless communication

andrekf,

 

You can use the RAIL: Simple TRX example. the array named data[] stores the values to be sent, you can replace with the character values you want to transmit. The example sends the packet when a button is pressed. You need to modify this to use a timer instead to trigger the start of the transmission.

 

Regards,

Imre