Reply
Posts: 11
Registered: ‎09-25-2016

EFR32 802.15.4 ADDRESS FILTER

[ Edited ]

Hi all ,

I met one problem when using EFR32FG IEEE802.15.4.

I can receive 802.15.4 data now, but can not filter address.

My code:

 

uint8_t longAddress[8] = { 0x11, 0x22, 0x33, 0x44,
0x55, 0x66, 0x77, 0x88};

RAIL_IEEE802154_AddrConfig_t nodeAddress = { 0x1234, 0x5678,
&longAddress[0] };
status = RAIL_IEEE802154_SetAddresses(&nodeAddress);

/* Configure 802.15.4 structure */
RAIL_IEEE802154_Config_t config = { false, false,
RAIL_IEEE802154_ACCEPT_STANDARD_FRAMES,
RAIL_RF_STATE_RX, 100, 192, 894, &nodeAddress };
/* Init RAIL => this also initalize ACK sending and address filtering */
if ( RAIL_STATUS_NO_ERROR != RAIL_IEEE802154_2p4GHzRadioConfig())
{
return 1;
}
if ( RAIL_STATUS_NO_ERROR != RAIL_IEEE802154_Init(&config))
{
return 1;
}

// Initialize Radio
RAIL_RfInit(&railInitParams);

// Initialize Radio Calibrations
RAIL_CalInit(&railCalInitParams);

// Configure modem, packet handler
changeRadioConfig(currentConfig);

// Configure RAIL callbacks with no appended info
RAIL_RxConfig(( RAIL_RX_CONFIG_FRAME_ERROR
| RAIL_RX_CONFIG_SYNC1_DETECT
| RAIL_RX_CONFIG_SYNC2_DETECT
| RAIL_RX_CONFIG_ADDRESS_FILTERED
| RAIL_RX_CONFIG_BUFFER_OVERFLOW
| RAIL_RX_CONFIG_BUFFER_UNDERFLOW
| RAIL_RX_CONFIG_SCHEDULED_RX_END
| RAIL_RX_CONFIG_PACKET_ABORTED),
true );
RAIL_TxConfig( RAIL_TX_CONFIG_BUFFER_UNDERFLOW
| RAIL_TX_CONFIG_BUFFER_OVERFLOW
| RAIL_TX_CONFIG_TX_ABORTED
| RAIL_TX_CONFIG_TX_BLOCKED
| RAIL_TX_CONFIG_CHANNEL_BUSY
| RAIL_TX_CONFIG_CHANNEL_CLEAR
| RAIL_TX_CONFIG_CCA_RETRY
| RAIL_TX_CONFIG_START_CCA);

RAIL_SetRxTransitions(RAIL_RF_STATE_RX, RAIL_RF_STATE_RX,
RAIL_IGNORE_NO_ERRORS);
RAIL_SetTxTransitions(RAIL_RF_STATE_RX, RAIL_RF_STATE_RX);

 

 

The code can receive any  channel 0 802.15.4 frame even I have set the address filter.

it will never go to RAIL_RX_CONFIG_ADDRESS_FILTERED;

 

 

/******************************************************************************
* RAIL Callback Implementation
*****************************************************************************/
void RAILCb_RxRadioStatusExt(uint32_t status)
{
if (status & RAIL_RX_CONFIG_FRAME_ERROR)
{
receivingPacket = false;
counters.frameError++;
LedToggle(1);
}
if (status & RAIL_RX_CONFIG_SYNC1_DETECT)
{
receivingPacket = true;
counters.syncDetect++;
rxFifoPrep();
if (abortRxDelay != 0) {
RAIL_TimerSet(abortRxDelay, RAIL_TIME_DELAY);
}
}
if (status & RAIL_RX_CONFIG_PREAMBLE_DETECT)
{
counters.preambleDetect++;
}
if (status & RAIL_RX_CONFIG_BUFFER_OVERFLOW)
{
receivingPacket = false;
counters.rxOfEvent++;
}
if (status & RAIL_RX_CONFIG_BUFFER_UNDERFLOW)
{
receivingPacket = false;
counters.rxUfEvent++;
}
if (status & RAIL_RX_CONFIG_ADDRESS_FILTERED)
{
receivingPacket = false;
counters.addrFilterEvent++;
}
if (status & RAIL_RX_CONFIG_RF_SENSED)
{
counters.rfSensedEvent++;
if (counters.rfSensedEvent == 0) // Wrap it to 1 not 0
{
counters.rfSensedEvent = 1;
}
}
if (status & RAIL_RX_CONFIG_PACKET_ABORTED)
{
counters.rxFail++;
}
// End scheduled receive mode if an appropriate end or error event is received
if ((status & RAIL_RX_CONFIG_SCHEDULED_RX_END)
|| ((schRxStopOnRxEvent && inAppMode(RX_SCHEDULED, NULL))
&& (status & RAIL_RX_CONFIG_ADDRESS_FILTERED
|| status & RAIL_RX_CONFIG_BUFFER_OVERFLOW
|| status & RAIL_RX_CONFIG_FRAME_ERROR)))
{
enableAppMode(RX_SCHEDULED, false, NULL);
}
}

 

Please help!   any sample code about address filter 802.15.4.

Posts: 34
Registered: ‎12-02-2016

Re: EFR32 802.15.4 ADDRESS FILTER

Hi,

Is the sequence of the code you put on the comment the orginal sequence in your project?

It's not suggested to reconfigure radio such as initializing or other configuration which is determined by 802.15.4 after enabling configuration about 802.15.4.  If do it, some features configured by calling 802.15.4 api may be changed so that they will not work well.

So, please move the part of configuring 802.15.4 after pre-initializing configuration of radio like below. And, let me know if it'll work well or not.

code :

1. power-on

2. pre-initialize radio

3. configurate 802.15.4 by calling the related API in a recommended sequence such as RAIL_IEEE802154_2p4GHzRadioConfig(), RAIL_IEEE802154_Init(), or calling other api to change address, panid or how to accept different frames.