Reply
Posts: 2
Registered: ‎06-06-2016
Accepted Solution

Connect Application for EFR32MG1P232F256GM48

My board package, BRD4151A [EFR32MG 2.4GHz 19.5 dBm], is not one of the selections available to create or build a Connect Framework sample all. Other MG selections are available but do not result in a working application, specifically the sensor app. This board is available from the solutions tab, but when create a project, the board selection is still not available. What is process to get this configuration available?

Posts: 267
Registered: ‎02-14-2014

Re: Connect Application for EFR32MG1P232F256GM48

Hi,

 

Support of your board was introduced in the latest Studio update, released today. Please install the update, the latest SDK that contains the Connect stack is called Gecko SDK suite. Let me know if it solves the issue.

Regards,
Tamás
Silicon Labs
Highlighted
Posts: 2
Registered: ‎06-06-2016

Re: Connect Application for EFR32MG1P232F256GM48

Hi Tamas, after update, the board selection is available and I can build and run. Of note, after the update, the source files change from connect-xxx.c to flex-xxx.c  e.g. connect-callbacks -> flex-callbacks. FYI. The Sensor sample still fails in the same way, but I will research this more before open new topic. Thanks for your help.