Recommended distance between antennas in an antenna diversity application

by <a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> dasimon on ‎11-25-2016 05:20 AM

Question

What is the recommended distance between antennas in an antenna diversity application?

Answer

Antennas in a product that implements antenna diversity have their antennas mounted at a distance of at least ¼ wavelength apart. This amount of spatial separation improves the probability that at least one antenna is NOT in a deeply faded signal condition. Another typical recommendation is ½ wavelength antenna distance, however, it can result quite large board sizes at low frequencies (e.g. for 434 MHz frequency ½ wavelength is 34,5 cm).