Reply
Highlighted
Posts: 2,955
Registered: ‎08-25-2015

WGM110: The Tweeting Gecko Wi-Fi Module

Introduction

 

This project is a follow up of the IFTTT article which instructed how to setup an IFTTT recipe and add a row to a google docs spreadsheet by sending an HTTP POST request from the Wizard Gecko WGM110 Wi-Fi Module.

 

On that example there was no additional data being sent on the HTTP request but on this project we will go one step further and add a JSON body to the request containing temperature and humidity data.

 

The temperature and humidity data are read from the Si7021 temperature and humidity sensor on-board the WSTK through I2C. The request is sent by pushing PB0 on the WSTK.

 

 

IFTTT Recipe

 

Please refer to IFTTT article mentioned in the introduction to learn how to create a recipe. To run this example you have to create a recipe and select the Twitter channel for "this" (don't forget to connect Twitter to your IFTTT account first) and then select chose "Post a tweet" as the action. You are free to write any text for the tweet and that includes adding up to 3 values which can be sent in the HTTP request.

 

For this project we created a Wizard Gecko Twitter account and using the recipe below the module is tweeting the temperature and humidity of our office in Espoo, Finland.

 

1.png

 

 

Adding the JSON body

 

For adding the data in JSON format we based on the implementation from the 'sensor' example of the WGM110 SDK.

 

# Procedure for creating the JSON data body
export procedure build_response_data()
	# Generate a response
	request_data_len = 0

	call api_add_json_object_start()
	# Temperature name
	call api_add_json_object_name(API_PARAM_JSON_TEMPERATURE_LEN, API_PARAM_JSON_TEMPERATURE(:))
	# Temperature value
	call api_add_json_integer(i2c_temperature)

	# adding a comma between JSON object element
	call api_add_comma()
	# Humidity name
	call api_add_json_object_name(API_PARAM_JSON_HUMIDITY_LEN, API_PARAM_JSON_HUMIDITY(:))
	# Humidity value
	call api_add_json_integer(i2c_humidity)
	# JSON status object end
	call api_add_json_object_end()
	
	call api_add_crlf()
	call api_add_crlf()
end

 

The full HTTP request is bellow where 'tt' and 'hh' are the temperature and humidity values respectively.

 

POST /trigger/YOUR_EVENT/with/key/YOUR_KEY HTTP/1.1\r\n
Host: maker.ifttt.com
Accept: */*
Content-Length: 26
Content-Type: application/json

{"value1":tt,"value2":hh}

 

 

Final Result

 

Press PB0 -> LED1 goes on -> LED1 goes off -> Tweet

 

original.gif