Reply
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Hero Employee</font></font> </a> Alf
Posts: 280
Registered: ‎09-06-2012

Using Arduino shields on EFM32 and EFR32 Silicon Labs Starter Kits

[ Edited ]

Arduino shields come in hand from time to time when you want to prototype some hardware.

 

As I had a Grove Base Shield from Seeed Studios I decided to give it a try to hack it together with one of our STKs and it actually turns out that this is possible. 

 

The unfortunate candidate to receive surgery this time, was a Mighty Gecko WSTK. All the newer starter kits have the correct spacing between the rows, it was just a matter of getting the pin mapping right. This is what I ended up with. The green dots are where headers will be added, and the red stars are pins on the Arduino shield that will have to be cut:

blue-gecko-dev-kit-blank_arduino.png

 

So I started by cutting the top three pins on the short side (NC, IOREF and RST). I also removed the 5V pin, as the shield will only communicate using 3.3V:

DSC_1775.JPG

 

Then you can see that the GND pins does not align properly. This was solved by grounding the pin next to it:

DSC_1772.JPG

 

As I have just created a Connected Coffe Machine and had a Grove LED Bar lying around I thought I'd upgrade the receiver with a nice LED bar, going from all green to full red when the coffee machine needs to be emptied. The code I used can be found here: https://github.com/SiliconLabsLabs/ConnectedCoffee

DSC_1774.jpg

 

Summary: You can use digital pins 0-7 and analog pins 0-5 on 3V Arduino shields with the Silicon Labs (W)STKs:

DSC_1772.JPG

My views are my own and do not necessarily represent the views of Silicon Labs
Posts: 48
Registered: ‎11-07-2015

Re: Using Arduino shields on Silicon Labs Starter Kits

Thanks for good article!

_____________________
Best regards,
Danil Borchevkin,
Owner Lab409.ru