Reply
<a href="http://community.silabs.com/t5/Welcome-and-Announcements/Community-Ranking-System-and-Recognition-Program/m-p/140490#U140490"><font color="#000000"><font size="2">Star</font></font> </a> PO
Posts: 1
Registered: ‎01-11-2017

School project involving the wstk bgm 111 and a LCD connected to a separate MCU

Hello, im fairly new to using BGscript and what im trying to do is program wstk bgm111 so it can communicate to a serial LCD screen.

I want to send send some information to the bgm111 from my phone then print it up on the LCD.(lcd-09394).

Is it possible? and if so anyone have any suggestions on were to start?

 

Im greatful for any help that i can get!