Reply
Highlighted
Posts: 4
Registered: ‎05-23-2016

ts1101

Hello,

 

I have problem with TS1101 if I use this current sensor and current is high frekvency, then SIGNAL pin is betwen 0 to 3 volt. Sometime is on 1,5 to 2,2V. VDD is corect 3V3, but CPU have problem with this. I use digital input. I measure current from lifepo batery 48V/ 100Ah to Victron DC/AC converter.

Can you help me with this?

 

Thank you.

Best regards

Pavel Musil

Posts: 4
Registered: ‎05-23-2016

ts1101

Hello,

 

I have problem with TS1101 if I use this current sensor and current is high frekvency, then SIGNAL pin is betwen 0 to 3 volt. Sometime is on 1,5 to 2,2V. VDD is corect 3V3, but CPU have problem with this. I use digital input. I measure current from lifepo batery 48V/ 100Ah to Victron DC/AC converter.

 

Can you help me with this?

 

Thank you.

Best regards

Pavel Musil

Posts: 29
Registered: ‎06-10-2015

Re: ts1101

The SIGN output is a digital HIGH for current from RS+ to RS-, and LOW  for current from RS- to RS+ (or for Load-disconnect). If the converter is pulling current  in the positive direction (VRS+ > VRS-) then stopping (VRS+ = VRS-), the SIGN pin should toggle between high and low. 

Posts: 4
Registered: ‎05-23-2016

Re: ts1101

Yes I know this, normaly work this, but if charge or discharke isnt DC (it is DC with HF AC) then SIGN is betwen 0,5 - 2,5V. If I instal kapacity on SIGN 10uF sometimes help but sometimes not.

Posts: 4
Registered: ‎05-23-2016

Re: ts1101

Now I see on osciloskop, cuent is DC with AC 50Hz superposition from DC/AC convertor. If convertor generate smal power everithing is ok, but if generate more then 200W, superposition is biger and SIGN pin is betwen 0.5 to 2,5 V.

Posts: 29
Registered: ‎06-10-2015

Re: ts1101

The SIGN output is dependent upon if VRS+ is greater than VRS-. There is a delay of 3msec if Vsense is +/-1mV. If SIGN is transitioning between GND and VDD it is because the voltage across VRS+ and VRS- is transient. Please use the oscilloscope to measure Vsense with respect to SIGN. SIGN will transition between HIGH and LOW depending upon Vsense.