Reply
Highlighted
Posts: 3
Registered: ‎03-29-2017

si4688 firmware package

I am looking for the (preferably latest) version of the si4688 firmware. I've seen people mentioning v5.0.7. There are some links on the forum but they are expired.

 

Can anyone help me? I couldn't find any other source.

Thanks!

Posts: 6
Registered: ‎08-01-2013

Re: si4688 firmware package

Hello,

 

Are you interested in both HD-Radio and DAB/DAB+?

 

If you are only interested in DAB please use Si4684 instead of Si4688.

 

HD-Radio requires a license so we cannot release the firmware until we get confirmation that you are working with DTS/iBiquity. Can you kindly let me know?

 

Regards

Abhijit

Posts: 3
Registered: ‎03-29-2017

Re: si4688 firmware package

Dear Abhijit,

 

Thank you for your reply!

 

I currently have a PCBA with the Si4688 on it and I can successfully activate the bootloader. The Si4688 was the only version that could be shipped in low quantity from Arrow USA.

I am mainly interested in the DAB/DAB+ and FM support. HD radio is not supported in my area (Netherlands).

 

Is there a firmware binary with DAB/DAB+ and FM support? Or a binary with HD Radio support disabled?

 

Thanks a lot! Much appreciated Robot Happy

 

Best Regards,

Johan

Posts: 6
Registered: ‎08-01-2013

Re: si4688 firmware package

Hi Johan,

 

Can you kindly provide your email address?

 

Thanks

Abhijit

Posts: 64
Registered: ‎02-15-2015

Re: si4688 firmware package

Hi Abhijit,

 

I am using the Si4684 and Si4685 and I am targeting the European market, so HD is not required (only FM, AM and DAB+).

Can you please also provide me the current firmware and documentation package?

 

Best regards,

Andi

Posts: 2,801
Registered: ‎02-07-2002

Re: si4688 firmware package

When you require someones personal email address, it´s better to send a private message through the forum instead of asking for it in the public forum. Any bot would pick it up from the forum and start sending you spam.

Posts: 3
Registered: ‎03-29-2017

Re: si4688 firmware package

To notify anyone reading here, I did actually send a private message, patiently waiting for a response Smiley Happy